See the Simulation Break Conditions section.
Field | Description |
---|---|
|
Opens the Help system. |
Add |
Use to add a break condition and opens the Break Conditions dialog box. |
Break Conditions Table | |
Rule | Displays existing break conditions. |
Active | The Active icon ( |
Enabled | Displays break conditions that are applied to the current simulation testing. |
|
Clicking the Trash icon deletes the break condition. |