Break Conditions - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Break conditions are conditions that you set up to prompt the simulation to automatically pause (break) if the system reaches the break condition. Setting up break conditions allows you to pause the simulation session based on your preset break conditions and view the status of your logic when the break condition is reached. By setting up break conditions, you can look at possible problems as they occur and troubleshoot programs as you write them. For example, you can set up a discharge air temperature to pause the simulation if the temperature exceeds 80 degrees. You can then view the point state or issue commands.