Binary Interlock Control - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The selection options for Binary Interlock Control are:

  • Use Existing BI (Manually Connect): This option does not load an Input, but allows the user to manually connect an existing Input to the Process Variable input of the selected control module.

  • Output Type

    • Binary Output

    • Analog Output

  • Delay Type

    • None

    • Delay when BI turns on

    • Delay when BI turns off

    • Delay when BI turns on and off