Analog to Binary Control - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The selection options for Analog to Binary Control are:

  • Input Type

    • Temperature

    • Humidity

    • Other: This option is configured by default for pressure control, but can be used for any generic input type.

  • Number of Inputs

    • Use Existing (Manually Connect): This option does not load an Input, but allows the user to manually connect an existing Input to the Process Variable input of the selected control module.

    • One

    • Two

      • Select Minimum Value

      • Select Maximum Value

      • Average Inputs

  • Control Action

    • Reverse Acting (for example, Heating, Supply Fan, and Humidifier)

    • Direct Acting (for example, Cooling and Exhaust Fan)