Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
About this task
To import System Selection preferences:
Procedure
In the Preferences - System Selection screen, select the System Selection tree that matches the type you want to import.
Click Import. The Open dialog box appears.
Select the desired file to import.
Note: You may need to browse to the location where you saved the file if you saved it to a different location from the default, or received the file from others.
Click Open. The preferences file opens and populates the System Selection preferences tree.