Importing Naming and Signal Preferences - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. Click Import. The Open dialog box appears.
  2. Select the object properties file to import. The default file name is ObjectNaming.properties.
    Note: You may need to browse to the location where you saved the file if you saved it to a different location from the default or received the file from others.
  3. Click Open. The preferences file opens and populates the Naming and Signal Preferences screen.