Exporting System Selection Preferences - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. In the Preferences - System Selection screen, select the System Selection tree that you want to export.
  2. Click Export. The Save dialog box appears.
  3. Keep the default file name of [application].properties or adjust the name to indicate a specific site or use.
    Notes:
    • The default file name for each selection tree is listed in the Import and Export Preferences section ([applicationname].properties).
    • It is not necessary to export/save a separate copy of the Johnson Controls standard preferences because the Reset function resets the preferences of the displayed selection tree to the Johnson Controls standard default values regardless of user session.
  4. Keep the default location to save the file or adjust it as desired.
    Note: The default location is C:\ProgramData\Johnson Controls\MetasysIII\<Product Name>\Configuration\Backup\SelectionTree
  5. Click Save. The file saves and you can access it from the same computer for later use or you can copy the file to use on another computer.