English (United States) is the default language used by the tool UI. A base translation of the other languages is provided (see Localization Preferences). You can use the localization preferences as an environment to translate the other languages listed in the Languages tab.
See Setting Localization Preferences.
|
Field |
Description |
|---|---|
|
Localization Tab |
Displays a list of the locales available, and allows you to choose the language the tool UI uses. The locales listed on this tab are defined on the Languages tab. Use to set a chosen language as the default language when you select the Use Default Language When Any CAF is opened (Ignore CAF Language) check box. Note: When changing the locale for the first time, additional localization data must be loaded. Prior to building any applications, restart the tool.
|
|
Naming Tab |
Note: When changing the locale for the first time, additional localization data must be loaded. Prior to building any applications, restart the tool.
Use to enter text in the desired language for the English text in the tool. For example, for Exhaust Filter, you can enter text in another language that should appear in place of the English text. The table in this tab has the following columns:
|
|
Systems Tab |
Use to enter text in the desired language for the English text in the tool. For example, for Rooftop Unit, you can enter text in another language that should appear in place of the English text. The table in this tab has the following columns:
|
|
Views |
Use to enter text in the desired language for the English text in the tool. For example, for Device Type, you can enter text in another language that should appear in place of the English text. The table in this tab has the following columns:
|
|
Selection Trees |
Use to enter text in the desired language for the English text in the System Selection trees. For example, for Device Type, you can enter text in another language that should appear in place of the English text. This tab has a navigation tree in the left pane of all the system selection trees (for example, Fan Coil) to select the context. The right pane has a table with the following columns:
|
|
Languages Tab |
Use to define the locale settings for the tool UI. The table in this tab has the following columns:
|
|
Local Display Dictionary Tab |
Use to enter text in the desired language for the English text in the tool dictionary (enumeration sets). This tab includes only those enumeration sets typically used by the display. The table in this tab has the following columns:
|
|
UI Resources Tab |
Use to enter text for items in the tool UI (buttons, messages, and dialog box names, for example) in the desired language. For example, to change the name of the Configure button, you can enter text in another language that should appear in place of the English text in the button.configure row. The table in this tab has the following columns:
|
|
Reset All |
Resets all values to the defaults. |
|
Import |
Opens a saved preference file and populates the screen with its data. See the Import and Export Preferences section. |
|
Export |
Saves preferences to a file so you can access it from the same computer for later use or you can copy the file to use on another computer. See the Import and Export Preferences section. |
|
Save |
Applies the changes and closes the screen. |
|
Close |
Closes the screen. If you did not save your changes, a dialog box appears asking if you want to save them before closing the screen. |
|
|
Opens the Help system. |