Module Use in Applications (Last Value) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual Setpoint Determination/Misc Last Value modules in this group using the names in Table 1.

Table 1. Last Value (Boolean, Enum, Float) Uses in Application System Selection Trees

Module Instance Name

Applications

2 Pipe Pump x MS LV (where x = 1 or 2)

All Air Handling Unit Applications

Autocalibrate Now LV

All VAV Applications

CD Area LV

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

CD Pickup Gain LV

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

CHW Cap Fault LV

Central Cooling with Optimization Applications

Central Cooling Applications

CHW Chlr Add OK LV

Central Cooling with Optimization Applications

Central Cooling Applications

Cooling Pump x MS LV (where x = 1 or 2)

All Air Handling Unit Applications

CW Cap Fault LV

Central Cooling with Optimization Applications

Central Cooling Applications

CW Chlr Add OK LV

Central Cooling with Optimization Applications

Central Cooling Applications

CW Pump Shed OK LV

Central Cooling with Optimization Applications

Central Cooling Applications

Exhaust Area LV

All VAV Applications

Exhaust Pickup Gain LV

All VAV Applications

HD Area LV

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

HD Pickup Gain LV

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

Preheat Pump x MS LV (where x = 1 or 2)

All Air Handling Unit Applications

Reheat Pump x MS LV (where x = 1 or 2)

All Air Handling Unit Applications

Supply Area LV

All VAV Applications

Supply Pickup Gain LV

All VAV Applications

To see a module's connections and how modules interact with it, view the Connections table.