Module Use in Applications (Status AND) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by this module:

Table 1. Status AND Uses in Application System Selection Trees
Module Instance Name Application
Pump Status AND Custom and Monitoring Supervisory Control Only Applications

To see a module's connections and how modules interact with it, view the Connections table.