The following table describes the attributes used by this module:
| Name | Type 1 | Description | Default Value |
|---|---|---|---|
| Any Off | Provides a Boolean value that indicates any input is off. | False | |
| All On | Provides a Boolean value that indicates all inputs are on. | False | |
| Cascaded AND Input |
Provides, as an input, the Cascaded AND Status from an additional module. |
On
Set Name: Off/On |
|
| Device X Status (Where x is 1–8) |
Provides, as an input, the binary status for up to 8 devices. |
On
Set Name: Off/On |
|
| Status AND | G |
Indicates the output of the module. When all inputs are ON, this output is ON. |
Off
Set Name: Off/On |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)