Attributes (Status AND) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by this module:

Table 1. Status AND Attributes
Name Type 1 Description Default Value
Any Off   Provides a Boolean value that indicates any input is off. False
All On   Provides a Boolean value that indicates all inputs are on. False
Cascaded AND Input  

Provides, as an input, the Cascaded AND Status from an additional module.

On

Set Name: Off/On

Device X Status (Where x is 1–8)  

Provides, as an input, the binary status for up to 8 devices.

On

Set Name: Off/On

Status AND G

Indicates the output of the module. When all inputs are ON, this output is ON.

Off

Set Name: Off/On

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)