Sideloop Minimum Selector - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module selects the minimum value of the inputs to produce the output. The module accepts two inputs and outputs the minimum of the inputs. You can add more inputs to the module.

You can view and modify the modules in this group’s logic.

To see this module’s connections and how modules interact with it: