Module Use in Applications (VAV Dual Duct Variable Flow Endpoint Calculation) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in Table 1.

Table 1. VAV Dual Duct Variable Flow Endpoint Calculation Uses in Application System Selection Trees

Module Instance Name

Applications

Standard Dual Duct Endpoint Calculation

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.