Attributes (VAV Dual Duct Constant Flow Endpoint Calculation) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Table 1 describes the attributes used by the VAV Dual Duct Constant Flow Endpoint Calculation modules.

Table 1. VAV Dual Duct Constant Flow Endpoint Calculation Attributes

Name

Type 1

Description

Default Value

Box Max Flow

 

Contains the constant flow for the dual duct box.

0 l/s, 0 cfm

CD Min Flow

 

Contains the minimum flow for the cold duct.

0 l/s, 0 cfm

EFFCD-MAXFLOW (Eff CD Max Flow)

V

Contains the effective maximum flow setpoint for the cold deck.

Display Units: l/s, cfm

EFFCD-MINFLOW (Eff CD Min Flow)

G, V

Contains the effective minimum flow setpoint for the cold deck.

Display Units: l/s, cfm

EFFHD-MAXFLOW (Eff HD Max Flow)

V

Contains the effective maximum flow setpoint for the hot deck.

Display Units: l/s, cfm

EFFHD-MINFLOW (Eff HD Min Flow)

V

Contains the effective minimum flow setpoint for the hot deck.

Display Units: l/s, cfm

HD Min Flow

 

Contains the minimum flow for the hot duct.

0 l/s, 0 cfm

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)