VAV Dual Duct Constant Flow Endpoint Calculation - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module is responsible for generating minimum and maximum deck flows for both the cold and hot decks of a constant volume dual duct application. The module accepts the minimum deck flow setpoints and the maximum box flow setpoint. The module outputs individual deck minimum and maximum flow setpoints.

You can view and modify the modules in this group’s logic.