Module Use in Applications (Summer Winter Compensation) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual module in this group using the names in Table 1.

Table 1. Summer Winter Compensation Uses in Application System Selection Trees

Module Instance Name

Applications

Summer Winter Compensation

AHU Mixed Air Single Duct Applications

AHU 100% Outdoor Air Single Duct Applications

AHU Rooftop Unit Applications

Fan Coil Applications

Heat Pump Applications

Unit Ventilator Applications

VAV Single Duct Applications

VAV Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.