Table 1 describes the attributes used by the Flow Differential Setpoint Calculation modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
EFFFLOW-DIFF (Diff Setpoint) |
G, V |
Contains the actual flow differential setpoint. |
Display Units: l/s, cfm |
|
OCCEAFLOW-DIFF (Occ Diff Setpoint) |
Contains the desired difference between the exhaust and supply flow or between the supply flow and return flow under occupied conditions. (Exhaust Flow-Supply Flow or Supply Flow-Return Flow). |
0 l/s, 0 cfm |
|
|
Occupancy |
Current Occupancy status of the unit. |
Unoccupied Set Name: Occ Effective |
|
|
UNOCCEAFLOW-DIFF (Unocc Diff Setpoint) |
Contains the desired difference between the exhaust and supply flow or between the supply flow and return flow under unoccupied and standby conditions. (Exhaust Flow-Supply Flow or Supply Flow-Return Flow). |
0 l/s, 0 cfm |