Table 1 describes the attributes used by the Discharge Air Setpoint Determination modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
DATCLGUNOCC-SP (Unocc Cooling Setpoint) |
Contains the Discharge Air setpoint used when unoccupied cooling or Cooldown is required. |
13 °C, 55 °F |
|
|
DATHTGUNOCC-SP (Unocc Heating Setpoint) |
Specifies the Discharge Air setpoint used when unoccupied heating or Warmup is required. |
32 °C, 90 °F |
|
|
EFFDAT-SP (Discharge Air Setpoint) |
G, V |
Indicates the effective Discharge Air Temperature Setpoint. |
13 °C, 55 °F |
|
Occ Setpoint |
Contains the Discharge Air setpoint used when unoccupied control and WarmupCooldown are not required. |
13 °C, 55 °F |
|
|
Unocc Status |
Current unocc status. This input indicates if unoccupied cooling, unoccupied heating, or neither is required. |
Unocc Ctrl Not Req’d Set Name: Unocc Status |
|
|
WarmupCooldown |
Indicates the current warm up or cool down status of the application. |
Normal Set Name: OST Warmup Cooldown |