Damper Minimum Position Determination - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module sets the minimum damper position to the Occ Min Damper Value when the Occupancy is Occupied or Bypass and sets it to zero otherwise.

You can view and modify the modules in this group’s logic.