Equipment Count - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Equipment Count module examines up to 16 enum inputs and indicates the total number of those inputs that have a status of ON, along with a status value if the total number of inputs ON exceeds the Minimum Running Devices input. The module accepts as inputs up to 16 ON/OFF inputs and the minimum number of devices required, and has outputs for the number of devices ON, a TRUE/FALSE state, and a status output.

This module is implemented as a Control Activity. You can view and modify the modules in this group’s logic.

Figure 1. Equipment Count Logic