Module Use in Applications (Equipment Count) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Equipment Count Uses in Application System Selection Trees

Module Instance Name

Application

Exhaust Fan Count

AHU 100% Outdoor Air Single Duct Applications

Relief Fan Count

AHU Mixed Air Single Duct Applications

Return Fan Count

AHU Mixed Air Single Duct Applications

Supply Fan Count

AHU Mixed Air Single Duct Applications

AHU 100% Outdoor Air Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.