Attributes (Equipment Count) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by this module:

Table 1. Equipment Count Attributes

Name

Type

Description

Default Value

Fan State

 

Indicates if more fans are ON than the defined minimum number of running devices using a Boolean value.

False

Fan Status

 

Indicates if more fans are ON than the defined minimum number of running devices using an enum output.

Off

Set Name: Off/On

Input n (where n is 1-16)

 

Provides the Binary status of each fan.

Off

Set Name: Off/On

Minimum Running Devices

G

Indicates the comparison threshold, where less than this number of fans is not considered ON for overall status.

1

Number of Devices Running

 

Indicates the number of inputs with a value of ON.

0

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)