Required Flow - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module is responsible for determining the required minimum flow setpoint for two pipe plants. This module accepts the inputs listed below. The module outputs either the cooling minimum flow or the heating minimum flow depending on the plant mode. It is implemented as a standard Control Activity.