Minimum Flow Calculation - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Minimum Flow Calculation module provides a minimum flow value based on the number of running devices. This module provides a float output. Based on the inputs, the module sets the Output equal to the Min Flow or the sum of the devices currently running, whichever is larger.