Table 1 describes the attributes used by the Flow Sum Calculation module.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Contributing Flow 1 |
Measured flow to be added to Contributing Flow 2. |
0 l/s, 0 cfm |
|
|
Contributing Flow 2 |
Measured flow to be added to Contributing Flow 1. |
0 l/s, 0 cfm |
|
|
DA-F, SA-F, or FLOW (Calculated Flow) |
G, V |
Contains the result of the addition with reliability. |
Display Units: l/s, cfm |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), DC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)