Reliability (Flow Calculation) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Reliability of the Flow Calculation module and its outputs is set as follows:

  • Input Unreliable: Set if either the Autocalibrate Now or Differential Pressure inputs are unreliable.

  • Math Error: Set if the external Patm (atmospheric pressure) function called by this module is unreliable.

  • Reliable: Set otherwise.