Module Use in Applications (Unocc Cooling Fan Lockout) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the Unocc Cooling Fan Lockout module in this group using the name in Table 1.

Table 1. Unocc Cooling Fan Lockout Uses in Application System Selection Trees

Module Instance Name

Applications

Unocc Cooling Fan Lockout

All Air Handling Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.