Table 1 describes the attributes used by the Unocc Cooling Fan Lockout module.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Cooling isAvailable |
Provides a network input used to enable or disable cooling. |
False |
|
|
Cooling Required |
Indicates whether there is a need for cooling. |
True |
|
|
Occupancy |
Indicates the effective occupancy command. |
Occupied Set Name: Occ Effective |
|
|
Present Value |
Indicates the current status of the device availability. The Present Value is True when the device is available and False when the device is not available. |
False |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)