Reliability (WarmupCooldown Determination) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Table 1. WarmupCooldown Determination Reliability

Input

Behavior When Input Is Not Reliable

Supply Air Temperature

Automatic Warmup activation is disabled and the module only passes through the network warmupcooldown mode input.

Zone Temperature

Automatic Warmup activation is disabled and the module only passes through the network warmupcooldown mode input.