Status Alarm Determination - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module generates the appropriate alarm state for a device. The Status Alarm Determination module monitors the command and flow status to determine whether the current state is Normal or Alarm. For information on how the FSM determines the state, see FSM (Status Alarm Determination).

You can view and modify the modules in this group’s logic.