Staged Device Enable Determination Series - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module generates the True, False, or Fault state to indicate to a staged device that the airflow requirements have been met. If either the fan command (on/off) is on or the supply flow is greater than the minimum flow value, the state is True. This module is designed for use with VAV boxes that contain a heating coil in the discharge air stream (series). This module can be used for VAV boxes with or without a fan. If a fan does not exist, the default Fan Mode value is Off and the default for the State does not change if the Fan Mode is not connected.

You can view and modify the modules in this group’s logic.