Table 1 describes the attributes used by the Flow Status Determination module.
|
Name |
Description |
Default Value |
|---|---|---|
|
Air Proving Switch |
Current status of the Air Proving Switch. |
Off Set Name: Off/On |
|
Delay |
Specifies the delay allowed for the fan to start before a fault occurs. |
30 Seconds |
|
Fan Mode |
Provides the last command sent to the fan. |
Off Set Name: Off/On |
|
Fan Status |
Current effective status of the Airflow Proving Switch. This attribute is the same as the Status except that Fault is mapped to False. |
|
|
FLOW-S (Status) |
Current effective status of the Airflow Proving switch. |
Set Name: False/True/Fault |