Attributes (Dual Fan Speed High Select) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by the Dual Fan Speed High Select modules.

Table 1. Dual Fan Speed High Select Common Attributes

Name 1

Type 2

Description

Default Value

Input 1

 

Indicates the float variable that is compared to other inputs.

0

Display Units: None

Input 2

 

Indicates the float variable that is compared to other inputs.

0

Display Units: None

Fan Percent Cmd

G

Indicates the result of the high select.

0.0

Display Units: None

1 Attributes apply to all the modules within this category.
2 B: BACnet Exposed Parameter, C: Configuration Mode Only, G: Default Element (Generated State, if applicable), SC: Simulation and Commissioning Modes Only, V: Calculated Value (Outputs)