Device Enable - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Device Enable group provides the ability to enable devices based on network commands or outdoor air temperature.

These modules are included in the Miscellaneous category because they typically, but not always, provide information to other State Generation modules rather than connecting directly to State Selection. Also, see the Device Enable category of modules in the State Generation Modules (State Generators) section.