Module Use in Applications (Waterside Economizer Suitability) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Waterside Economizer Uses in Application System Selection Trees

Module Instance Name

Applications

Waterside Economizer Suitability

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.