The following table describes the attributes used by this module:
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
O3 |
Provides a Boolean output value that indicates all inputs are OFF. |
False |
|
|
O2 |
Provides a Boolean output value that indicates whether any input is ON. |
False |
|
|
Cascaded OR Input |
Provides, as an input, the Cascaded OR Status from an additional module. |
False |
|
|
Device X Status (Where X is 1-8) |
Provides, as an input, the binary status for up to 8 devices. |
Off Set Name: Off/On |
|
|
Status - OR |
G |
Indicates the output of the module. When any input is ON, this output is ON. |
Off Set Name: Off/On |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)