Attributes (Status OR) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by this module:

Table 1. Status OR Attributes

Name

Type 1

Description

Default Value

O3

 

Provides a Boolean output value that indicates all inputs are OFF.

False

O2

 

Provides a Boolean output value that indicates whether any input is ON.

False

Cascaded OR Input

 

Provides, as an input, the Cascaded OR Status from an additional module.

False

Device X Status (Where X is 1-8)

 

Provides, as an input, the binary status for up to 8 devices.

Off

Set Name: Off/On

Status - OR

G

Indicates the output of the module. When any input is ON, this output is ON.

Off

Set Name: Off/On

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)