Load Filter - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Load Filter module provides a digital filtered value for use within a Control Sequence.

The module has four main inputs:

  • Enable: When True, the Filter calculates a digital filtered value for the output after the Startup Delay time passes. When False, the input passes directly to the output.
  • Filter Enable: When On, the Filter calculates a digital filtered value for the output. When Off, the input passes directly to the output.
  • Input: Provides a floating point value and is typically connected from another block.
  • Time Constant: Determines the cutoff frequency and the execution period.

You can view and modify the modules in this group’s logic.