Flow Direction Determination - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Some flow sensors measure the absolute value of flow and do not indicate the flow direction. If this type of sensor is used in the central plant application, you must use another sensor to measure the flow polarity. This module merges the direction and flow into one value. This module has inputs for the flow Direction and Flow value, and a single signed output for the flow value.

You can view and modify the modules in this group’s logic.