Module Use in Applications (Capacity Calculation) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Capacity Calculation Uses in Application System Selection Trees

Module Instance Name

Application

Capacity Calculation Amp XX

(Where XX is 01-08)

Central Cooling with Optimization Applications

Capacity Calculation Pct FLA X

(Where XX is 01-08)

Central Cooling with Optimization Applications

Chiller Load Total Calc Amps

Central Cooling with Optimization Applications

Chiller Load Total Calc Pct Amps

Central Cooling with Optimization Applications

CHW Pump Capacity Check X

(Where X is 1-8)

Central Cooling with Optimization Applications

CW Pump Capacity Check X

(Where X is 1-8)

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.