The following table describes the attributes used by the Alarm OR modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Alarm |
Provides a Boolean output value that indicates if any input is in Alarm. |
False |
|
|
Alarm - OR |
G, V |
Indicates the output of the module. When any input is in Alarm, this output is in Alarm. |
Normal Set Name: Normal/Alarm |
|
Cascaded OR Input |
Provides, as an input, the Cascaded OR Alarm from an additional module. |
Normal Set Name: Normal/Alarm |
|
|
Device X Alarm (Where X is 1-8) |
Provides, as an input, the binary alarm for up to 8 devices. |
Normal Set Name: Normal/Alarm |
|
|
Normal |
V |
Provides a Boolean output value that indicates all inputs are Normal. |
False |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)