Configuring Associated Perspectives for All Applications - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. In the Perspective Management window, click the System Configurations tab.
  2. In the left pane, select All System Configurations.
  3. In the right pane, select or clear the check boxes for the perspectives that you want available for each application. You can also right-click a perspective or a column heading and click Select All or Deselect All.
    Note: Perspectives are listed in alphabetical order. To reverse the order, click the Perspective column heading.
  4. Once you have completed your selections, click Close.