Adding a Container - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. Click Settings and select Perspective Management. The Perspective Management window appears.
  2. In the tree on the left pane, select the perspective or container to which you want to add the container. The container you add becomes a subcomponent of the perspective component you choose.
    Note: You cannot add containers to widgets.
  3. Click Add Container ().
  4. Select Orientation or Tab. The container appears nested under the component you selected in 2.
    Note: If you decide later that you want a different type container, you can switch your choice for Orientation or Tab type at any time for the container you added. You do not need to delete the container and add a new container.
  5. See Configuring a Tab Container or Configuring an Orientation Container for more information.