Connections - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Connections table appears in the Connection tab of the Features Panel in all modes. This table can show the connections for one or more modules and the State Selection tables. The Connections table displays the source and destination module and port data with the associated input and output connection of the selected module. In this table, inputs appear yellow and outputs appear turquoise.

In the Control tab, you can select to view connections for one module, multiple modules in a module category, State Selector only, or you can click Show All to view all connections.

In the Logic tab, you can select a module in the Activities tree to view the connections for the selected module. You can also select a module in the BACnet Exposed tab to view and update the Connections table.

Note: Select the Freeze Connection check box to prevent the Connections table from dynamically changing as you select modules.
Figure 1. Connections Table Show All Menu

For Inputs and Outputs, the default value appears after the input/output name during Configuration mode (for example, Present Value - False or Input - False). During Simulation and Commissioning mode, the current value/present value appears after the input/output name. The following table describes the right-click menu options of the Connections table.

Table 1. Connections Table Right-Click Menus

Menu Option

Context

Description

Break Connection

Input

Output

Disconnects the current connection and leaves the connection blank.

Change Connection

Input

Output

Launches a dialog box allowing the user to choose from a tree of available blocks and ports.

Expose Ports

Selected Module Header

Opens the Port Exposure dialog box to show or hide ports from connection. You cannot remove the selection for connected ports as such ports are disabled in this dialog box.

Make Connection

Input

Output

Launches a dialog box allowing the user to choose from a tree of available blocks and ports.

Table 2. Connections Table Buttons and Check Boxes

Button or Check Box

Description

Show All

Returns the Connections table to the default view, which is showing all module connections.

Show State Selector When selected, this option shows only the State Selector.

Expose Ports

Opens the Port Exposure dialog box to hide ports from connection. You cannot remove the selection for connected ports as such ports are disabled in this dialog box.

Freeze Connections

Prevents the Connections table from dynamically changing as you select modules.

See the Features Panel Screen section for a description of this table’s components.