Advanced Data - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Advanced tab allows you to view and configure advanced program features, such as controller information, intrinsic alarming, schedules, calendars, and trends.

Different trees and features appear on the Advanced tab depending on if the controller is an Advanced Application, General Purpose, or VAV Controller.

The Device Information folder provides access to device information. Device information can be viewed and edited by clicking on the device name.

See the Configuring Advanced Controller Features section for details on using this tab.

Note: The Advanced Data widget does not show the N2 object. For information on Advanced data functionality, see Configuring Advanced Controller Features. For N2 information, see the N2 Compatibility Options section.