Frame - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Frame container is only available at the perspective (or root level) and specifies that the subcomponents of information appear as frames. The name of each frame stems from the name of the associated perspective subcomponent. For example, the Classic View is a root frame container that defines the Application and the Features panels as frames.