Container - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

When you build a perspective, containers allow you to organize the content according to specific properties. Container types include Frame, Orientation, and Tab. Each container type can be added individually. In addition, after adding a container, you can change the type to another type of container, such as switching an Orientation container to a Tab container.

Table 1. Container Types and Properties
Icon Description Properties
Indicates a Frame container, which can only be added at the root level.

Orientation

Indicates an Orientation container, which can be vertical or horizontal.

Orientation

Resizable

Visible

Indicates a Tab container, which can be positioned in various locations of the UI.

Position

Visible