Classic View Components - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following figure and tables show how the Classic View is broken into components of a perspective.

Figure 1. Classic View with Callouts

Table 1. General Perspective Components
Callout Perspective Component
1 Frame Container - Vertical
2 Tab Container
3 Orientation Container - Horizontal
4 System Information Details Data Widget - BACoid
5 Table Data Widget - UI Column
6 Orientation Container - Vertical
7 Perspective Name
Specialized, Non-configurable Widget
Table 2. Description of Classic View as Perspective Components
Classic View Component Type Orientation/ Location/ Data Criteria Direct Subcomponents Appearance Description
Entire Classic View Frame Container Vertical

Tab Container (Application)

Tab Container (Features)

The vertical orientation of this frame container orders the direct subcomponents to arrange themselves stacked vertically, so the Application Panel and Features Panel appear stacked on top of each other.
Application Panel Tab Container Top

Orientation Container - Horizontal (Control Tab)

Logic View Widget (Logic Tab)

The Tab Container type dictates that the direct subcomponents appear as tabs within this container. The Top orientation provides the location of the tabs within the container.
Control Tab Orientation Container Horizontal

Orientation Container (Inputs)

Table Data Widget - UI Column (Setpoint/Miscellaneous)

Table Data Widget - UI Column (State Generation)

Table Data Widget - UI Column (Output Control)

Orientation Container (Outputs)

The orientation container type specifies that the subcomponents appear horizontally, or next to each other in the UI.
Network Inputs, Inputs, Miscellaneous Column Orientation Container Vertical

Table Data Widget - UI Column (Network Inputs)

Table Data Widget - UI Column (Inputs)

Table Data Widget - UI Column (Miscellaneous)

The orientation container type specifies that the subcomponents appear vertically stacked in the UI.
Setpoint/ Miscellaneous Table Data Widget UI Column None The table data widget with UI Column data criteria specifies that Setpoint/Miscellaneous blocks appear in UI.
State Generation Table Data Widget UI Column None The table data widget with UI Column data criteria specifies that State Generation blocks appear in UI.
Output Control Table Data Widget UI Column None The table data widget with UI Column data criteria specifies that Output Control blocks appear in UI.
Network Outputs, Outputs, Miscellaneous Column Orientation Container Vertical

Table Data Widget - UI Column (Network Outputs Inputs)

Table Data Widget - UI Column (Outputs)

Table Data Widget - UI Column (Miscellaneous)

The orientation container type specifies that the subcomponents appear vertically stacked in the UI.
Logic Tab Logic View Widget Not Applicable None The Logic View widget is designed specifically for the Logic view.
Features Panel Tab Container Top

Parameters Widget

Connections Widget

State Tables Widget

Local Display Widget

Advanced Data Widget

BACnet Exposed Widget

The Tab Container type dictates that the direct subcomponents appear as tabs within this container. The Top orientation provides the location of the tabs within the container.
Parameters Tab Parameters Widget Not Applicable None The Parameters widget is designed specifically for viewing parameters.
Connections Tab Connections Widget Not Applicable None The Connections widget is designed specifically for viewing connections of the Control Sequence.
State Tables Tab State Tables Widget Not Applicable None The State Tables widget is designed specifically for viewing the state tables.
Display Tab Local Display Widget Not Applicable None The Local Display widget is designed specifically for viewing the configuration of the display device.
Advanced Tab Advanced Data Widget Not Applicable None The Advanced Data widget is designed specifically for the viewing Advanced details.
BACnet Exposed Tab BACnet Exposed Widget Not Applicable None The BACnet Exposed widget is designed specifically for viewing BACnet exposed data.