CCT/PCT Programming Troubleshooting - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Check for common problems with custom CCT/PCT Programming or modifications made to standard applications. Perform the following system checks:

  • Ensure that the correct Process ID is selected and allowed to control the system.
  • Ensure that the PID is not active when it does not have control of the output.
  • Check connections to the PID Pre-Processor to see what values it is set to use.
  • Check the PID Pre-Processor. If the Standard Tuning is set to True, the Process ID sets the tuning parameters. If not, the parameters set in the PID Pre-Processor are the tuning parameters.
  • Check connections between the PID Pre-Processor and the PID. If there is a connection for the parameter, the PID uses the value determined by the PID Pre-Processor. If there is no connection, it uses the parameter value set in the PID.
  • Check the PID.
    • Is Adaptive Tuning set to True?
    • Is Manual Tuning set to True?